adc using 12-bit Cyclic Analog-to-Digital Converter in MC56F84789

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adc using 12-bit Cyclic Analog-to-Digital Converter in MC56F84789

948 Views
josephxavier
Contributor III

can any one share a ADC program using 12-bit Cyclic Analog-to-Digital Converter in MC56F84789.

i just need to read and display the ADC  values

Labels (1)
0 Kudos
Reply
1 Reply

840 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello joseph

For 12bit ADC configuration, you can refer to this application note, it contains the initialization code for ADC A/B working in Simultaneous mode.

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4608.pdf

Hope this helps!

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply