about sci of dsc56f800e

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about sci of dsc56f800e

Jump to solution
1,477 Views
tonglimin
Contributor I

I used Processor Expert program,and I used SCI sending my  data,but It can not correct to send data in event when i used  AS1_SendBlock((byte*)&message, sizeof(message),  &Sent),but,it be used in main is correct.the DSC is 56F8006

Labels (1)
0 Kudos
Reply
1 Solution
1,359 Views
TICS_Fiona
NXP Employee
NXP Employee

Please move the SCI initialization code to main function, and avoid delay and while loop for status waiting in ISR. For details, please refer to your SR.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,360 Views
TICS_Fiona
NXP Employee
NXP Employee

Please move the SCI initialization code to main function, and avoid delay and while loop for status waiting in ISR. For details, please refer to your SR.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------