XGate and Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

XGate and Processor Expert

跳至解决方案
3,085 次查看
sricker
Contributor I
CW pro v4.6, Target 9S12XDP512
 
I am trying to get up to speed on XGate. Planning on making the switch from HCS12 so I started a new project in CW with XDP512 as the target. Why is processor expert suspended automatically? Adding it introduces lots of conflicts. Is processor expert going to be trouble to use with the XGate chip?
 
-shawn
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,350 次查看
CrasyCat
Specialist III
Hello
 
Processor Expert doesn't support the XGATE at this time.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,350 次查看
tim_milliken
Contributor III
I ran into the same issue. I assumed that PE does not support the X Gate, so there for they disabled it automaticly. And yes if you enable it after you start the project it will cause a ton of problems. Your best bet is to not use it, and if you need it make your self a "Junk" project for the regular DP512 and use PE on it and just copy over the code from one project to the other. ope this helps. Tim
0 项奖励
回复
1,351 次查看
CrasyCat
Specialist III
Hello
 
Processor Expert doesn't support the XGATE at this time.
 
CrasyCat
0 项奖励
回复