Why ??? CW 10.4 SE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why ??? CW 10.4 SE

2,124 次查看
thoomanwang
Contributor V

5859_5859.jpgcw104_e.jpg

标签 (1)
0 项奖励
回复
4 回复数

1,979 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

it would be good if you would describe your problem?

0 项奖励
回复

1,979 次查看
thoomanwang
Contributor V

In CW10.4 se New a FRDM-kl05z project, add GPIO bean, set the three ports ( see figure above ) , and then build all, in the console window prompt project is not compiled ,why ?

0 项奖励
回复

1,979 次查看
BlackNight
NXP Employee
NXP Employee

It looks like you already have built it (folder FLASH)?

Otherwise, if you changed the component settings, do not forget to generate code, so you have the new source files.

(that small icon in the components view with the red arrow):

pastedImage_0.png

I hope this helps.

0 项奖励
回复

1,979 次查看
thoomanwang
Contributor V

I viewed FLASH directory, file does not compile successfully , that elf file does not exist. I restarted CW10.4 after successful compilation , but I alone erasable ROM is successful writing tasks in the implementation of the system error , the error is the ROM erase error.

I feel CW10.x IDE exists a lot of problems , I am now very worried about my next development ( Next My company plans to develop Zigbee module , and MC1323x the zigbee codebase only supports CW10.x, I am now on whether to adopt Freescale's programs are increasingly hesitant ) .

I use CW10.4 import FRDM_kl05z Development Kit code , the compiler is always a problem , but not the same problems every time , do not know in the end where there is a problem .

0 项奖励
回复