Where is the ROM_LIB keyword generated .S19 file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the ROM_LIB keyword generated .S19 file?

Jump to solution
1,494 Views
bennyxu
Contributor I
LINK ROMLIB.lib AS ROM_LIB
 
generated .s19 file very small.
 
HOW to used to "ROM_LIB"
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
929 Views
CompilerGuru
NXP Employee
NXP Employee
Hi bennyxu,

AFAIK, there is nothing special about the SRecord generation with ROM libraries compared to the SRecord generation with "normally" linked applications.
Do you build from within the CW ide? If so, add a *.bbl file to your project, the SRecord ends up in the bin folder in the "normal" setup.
If you are building with a makefile, use the burner.exe to create an SRecord.

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
930 Views
CompilerGuru
NXP Employee
NXP Employee
Hi bennyxu,

AFAIK, there is nothing special about the SRecord generation with ROM libraries compared to the SRecord generation with "normally" linked applications.
Do you build from within the CW ide? If so, add a *.bbl file to your project, the SRecord ends up in the bin folder in the "normal" setup.
If you are building with a makefile, use the burner.exe to create an SRecord.

Daniel
0 Kudos
Reply