Where is the ROM_LIB keyword generated .S19 file?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where is the ROM_LIB keyword generated .S19 file?

跳至解决方案
1,519 次查看
bennyxu
Contributor I
LINK ROMLIB.lib AS ROM_LIB
 
generated .s19 file very small.
 
HOW to used to "ROM_LIB"
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
954 次查看
CompilerGuru
NXP Employee
NXP Employee
Hi bennyxu,

AFAIK, there is nothing special about the SRecord generation with ROM libraries compared to the SRecord generation with "normally" linked applications.
Do you build from within the CW ide? If so, add a *.bbl file to your project, the SRecord ends up in the bin folder in the "normal" setup.
If you are building with a makefile, use the burner.exe to create an SRecord.

Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
955 次查看
CompilerGuru
NXP Employee
NXP Employee
Hi bennyxu,

AFAIK, there is nothing special about the SRecord generation with ROM libraries compared to the SRecord generation with "normally" linked applications.
Do you build from within the CW ide? If so, add a *.bbl file to your project, the SRecord ends up in the bin folder in the "normal" setup.
If you are building with a makefile, use the burner.exe to create an SRecord.

Daniel
0 项奖励
回复