Where is MCUToolsBaseDir defined?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is MCUToolsBaseDir defined?

ソリューションへジャンプ
1,732件の閲覧回数
j___
Contributor IV

CodeWarrior 10.7.

 

I see "MCUToolsBaseDir" used in several places in the project. However, I cannot find where it is defined or aliased. I looked in "Linked Resources" in the "Project Properties" but it is not there. I searched the document "CodeWarrior Development Studio Common Features Guide, Rev. 10.x, 01/2016" and found no references to it. I grepped the project directory and found a few references in the ".cproject" file but they did not expand into the path information. It seems odd to have such a pervasive alias without clearly making available its translation?!!

 

So, where is the alias, "MCUToolsBaseDir", defined, resource linked, or documented?

EDIT: Changed text to reflect that this is not found in the ...Common Features Guide...

0 件の賞賛
返信
1 解決策
1,626件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

Please go to a project properties then follow attached steps in screenshot below

pastedImage_1.png
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,627件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

Please go to a project properties then follow attached steps in screenshot below

pastedImage_1.png
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信