Where can I get the technical notes?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I get the technical notes?

ソリューションへジャンプ
3,679件の閲覧回数
wangyanjun
Contributor II
Where can I download the technical notes? I'm using the Codewarrior for hcs12, and the manual list some technical notes number such as TN238, TN240. But I can't find them. Where can I get them. Thanks!
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,511件の閲覧回数
mayfly
Contributor III
I had quite a time trying to find the technical notes until I came upon this thread.  Tried googling and a search on freescale for the specific Technical note (tn100)...but nothing came up.   A bit frustrating...I think someone should fix that somewhere. 

Here's the direct link:
http://www.freescale.com/files/soft_dev_tools/doc/support_info/CW_816-bit_Technical_Notes_SP.exe?fps...

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,512件の閲覧回数
mayfly
Contributor III
I had quite a time trying to find the technical notes until I came upon this thread.  Tried googling and a search on freescale for the specific Technical note (tn100)...but nothing came up.   A bit frustrating...I think someone should fix that somewhere. 

Here's the direct link:
http://www.freescale.com/files/soft_dev_tools/doc/support_info/CW_816-bit_Technical_Notes_SP.exe?fps...
0 件の賞賛
返信
2,511件の閲覧回数
Lundin
Senior Contributor IV
When you installed CW there should have been an option to include them. Otherwise they can be found in pdf format on the CW cd.
0 件の賞賛
返信
2,511件の閲覧回数
CrasyCat
Specialist III
Hello
 
You can download the Technical Notes from the Web as follows:
 
  - Click on the link "HC(S)08/RS08 Microcontrollers"
  - Click on the tab "Documentation"
  - Click on the link "816TNSP"
 
You should then get the .zip file containing the technical notes.
 
CrasyCat
 
0 件の賞賛
返信