What development package kit (eva/dev board, emulator, CW, etc) do I need for MCF52255CAF80?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What development package kit (eva/dev board, emulator, CW, etc) do I need for MCF52255CAF80?

1,295件の閲覧回数
junhan
Contributor I

Hello,
I will develop a project based on coldfire MCU MCF52255CAF80.
I am trying to find a development package kit, includes evaluation/development board, emulator and development tool CodeWarrior.
But I am not sure whether they are right parts as the followings:
Evaluation Board: E52259EVB, E52259DEMOKIT, or TWR-MCF5225X
Emulator: USBMLCF, or USB-ML-CFE
Development Tool:  CodeWarrior ColdFire 7.2 (XP, or W7)

Some of them are no longer supoorted by freescale.

Could you give me any suggestions?

 

Thanks!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,071件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Jun han.

regarding to board,  i suggest you use TWR-MCF5225X, the other two boards you mentioned are old and we don't recommend.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-MCF5225X&fsrch=1

CodeWarrior ColdFire 7.2 , This product is a 32-bit application. if you use 64bit win7, we suggest you use CW0.6 instead, here it is:

https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH

Hope this helps!

==================================================================

this answer is for you, if it helps, please click on "Correct Answer"  button. Thanks!

Best Regards,

Zhang Jun

1,071件の閲覧回数
junhan
Contributor I

Thank you for your answers.  But

What is the right emulator for TWR-MCF5225X? and is the emulator supported by CodeWarrior 10.6 on Win7-64?
Thanks,

Jun Han

0 件の賞賛
返信