What debugger command could "open configuration" in Hi-wave?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What debugger command could "open configuration" in Hi-wave?

跳至解决方案
1,488 次查看
DanielTan
Contributor I

In Hi-wave, "File->Open Configuration" could a load a .ini file.

Could I use a debugger command in Command component to load a .ini file?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
947 次查看
CrasyCat
Specialist III

Hello

 

No you cannot load a configuration from command line component.

The configuration must be known when HI-WAVE is started.

 

Instead you can use option -Prod on the command line when starting HI-WAVE to specify the configuration (.ini file) you want to use.

 

Available command line options are listed in section "Command Line Options" in debugger manual.

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
948 次查看
CrasyCat
Specialist III

Hello

 

No you cannot load a configuration from command line component.

The configuration must be known when HI-WAVE is started.

 

Instead you can use option -Prod on the command line when starting HI-WAVE to specify the configuration (.ini file) you want to use.

 

Available command line options are listed in section "Command Line Options" in debugger manual.

 

CrasyCat

0 项奖励
回复