Urgent Help Needed with Debugger Command Scripts Assigning Values to Type double

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Urgent Help Needed with Debugger Command Scripts Assigning Values to Type double

跳至解决方案
1,959 次查看
marv
Contributor I
Greetings,
 
I am writing some command scripts for our verification process when I ran into a stumbling block.  In the script we need to set some variables to specific values and then execute the program.  Everything works pretty well, except I am unable to set program variables that are declared as type double.  I.e.,
 
double mumbo;
 
In the command script I have:
 
A mumbo = 0
 
or
 
A mumbo = 0.0
 
all generate the same error:
 
Error: unknown variable   ^

The ^ sign is placed after the equal sign in the expression and seems to point to an issue with the assignment.  Furthermore, I can examine the variable fine from the command script, so I think it recognizes the variables, but I can not assign any values to type double.

I tried doubles that are global and local and the results are the same, so it does not appear to be a scope issue.  I have structures that contain mixed types and I can set any member as long as it is not a double.

How do I do this?  We are just getting ready for verification of our program and are up against a schedule crunch.

 

Thanks in advance,

 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,286 次查看
CrasyCat
Specialist III
Hello
 
Try
     A mumbo= "0.0"
If this does not work, make sure the variable mumbo is a global variable and that it has been linked to the application.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,287 次查看
CrasyCat
Specialist III
Hello
 
Try
     A mumbo= "0.0"
If this does not work, make sure the variable mumbo is a global variable and that it has been linked to the application.
 
CrasyCat
0 项奖励
回复