Urgent Help Needed with Debugger Command Scripts Assigning Values to Type double

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Urgent Help Needed with Debugger Command Scripts Assigning Values to Type double

ソリューションへジャンプ
1,966件の閲覧回数
marv
Contributor I
Greetings,
 
I am writing some command scripts for our verification process when I ran into a stumbling block.  In the script we need to set some variables to specific values and then execute the program.  Everything works pretty well, except I am unable to set program variables that are declared as type double.  I.e.,
 
double mumbo;
 
In the command script I have:
 
A mumbo = 0
 
or
 
A mumbo = 0.0
 
all generate the same error:
 
Error: unknown variable   ^

The ^ sign is placed after the equal sign in the expression and seems to point to an issue with the assignment.  Furthermore, I can examine the variable fine from the command script, so I think it recognizes the variables, but I can not assign any values to type double.

I tried doubles that are global and local and the results are the same, so it does not appear to be a scope issue.  I have structures that contain mixed types and I can set any member as long as it is not a double.

How do I do this?  We are just getting ready for verification of our program and are up against a schedule crunch.

 

Thanks in advance,

 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,293件の閲覧回数
CrasyCat
Specialist III
Hello
 
Try
     A mumbo= "0.0"
If this does not work, make sure the variable mumbo is a global variable and that it has been linked to the application.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,294件の閲覧回数
CrasyCat
Specialist III
Hello
 
Try
     A mumbo= "0.0"
If this does not work, make sure the variable mumbo is a global variable and that it has been linked to the application.
 
CrasyCat
0 件の賞賛
返信