Two user in the same workspace

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two user in the same workspace

Jump to solution
2,621 Views
mBeppe
Contributor I

Hi

 

we want to use the same workspace (but different project)

 

But when the second user launches CodeWarrior 10.3 has an error message


"Could not launch the product because the associated workspaces is currently in use by another eclipse application"

 

exist a workaround for this problem ?

 

ciao, beppe

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,244 Views
BlackNight
NXP Employee
NXP Employee

Hello,

no, you cannot use the same workspace with two different users (or two different instances of Eclipse).

Because there are many files (cache files, history, etc) which are tight to the running instance.

But you can use one workspace for each user, and use the same (shared) projects: It is not needed that you have the projects inside the workspace folder.

I hope this helps.

View solution in original post

0 Kudos
Reply
2 Replies
2,244 Views
mBeppe
Contributor I

Erich

Perfect, work fine

ciao, beppe

0 Kudos
Reply
2,245 Views
BlackNight
NXP Employee
NXP Employee

Hello,

no, you cannot use the same workspace with two different users (or two different instances of Eclipse).

Because there are many files (cache files, history, etc) which are tight to the running instance.

But you can use one workspace for each user, and use the same (shared) projects: It is not needed that you have the projects inside the workspace folder.

I hope this helps.

0 Kudos
Reply