Two user in the same workspace

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Two user in the same workspace

跳至解决方案
2,681 次查看
mBeppe
Contributor I

Hi

 

we want to use the same workspace (but different project)

 

But when the second user launches CodeWarrior 10.3 has an error message


"Could not launch the product because the associated workspaces is currently in use by another eclipse application"

 

exist a workaround for this problem ?

 

ciao, beppe

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,304 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

no, you cannot use the same workspace with two different users (or two different instances of Eclipse).

Because there are many files (cache files, history, etc) which are tight to the running instance.

But you can use one workspace for each user, and use the same (shared) projects: It is not needed that you have the projects inside the workspace folder.

I hope this helps.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,304 次查看
mBeppe
Contributor I

Erich

Perfect, work fine

ciao, beppe

0 项奖励
回复
2,305 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

no, you cannot use the same workspace with two different users (or two different instances of Eclipse).

Because there are many files (cache files, history, etc) which are tight to the running instance.

But you can use one workspace for each user, and use the same (shared) projects: It is not needed that you have the projects inside the workspace folder.

I hope this helps.

0 项奖励
回复