Two user in the same workspace

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two user in the same workspace

ソリューションへジャンプ
1,703件の閲覧回数
mBeppe
Contributor I

Hi

 

we want to use the same workspace (but different project)

 

But when the second user launches CodeWarrior 10.3 has an error message


"Could not launch the product because the associated workspaces is currently in use by another eclipse application"

 

exist a workaround for this problem ?

 

ciao, beppe

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,326件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

no, you cannot use the same workspace with two different users (or two different instances of Eclipse).

Because there are many files (cache files, history, etc) which are tight to the running instance.

But you can use one workspace for each user, and use the same (shared) projects: It is not needed that you have the projects inside the workspace folder.

I hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,326件の閲覧回数
mBeppe
Contributor I

Erich

Perfect, work fine

ciao, beppe

0 件の賞賛
返信
1,327件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

no, you cannot use the same workspace with two different users (or two different instances of Eclipse).

Because there are many files (cache files, history, etc) which are tight to the running instance.

But you can use one workspace for each user, and use the same (shared) projects: It is not needed that you have the projects inside the workspace folder.

I hope this helps.

0 件の賞賛
返信