True Time Simulator Counting Breakpoints Not Working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

True Time Simulator Counting Breakpoints Not Working

跳至解决方案
2,576 次查看
GFSmith
Contributor II
Hello,
I'm working with a recent version of Freescale's CodeWarrior Development Studio,
version 5.7.0, build 2211, for the HCS12 processor, specifically the MC9S12E128,
and the True Time Simulator (Version 6.1, Build 6345).

Downloading code, single-stepping through the code, and setting simple
breakpoints is working.  I can't get Counting Breakpoints to work.  I have
followed the directions by setting the interval to say, for example, "4", then
running the code, but the debugger appears to be triggering as soon as it hits
the breakpoint instead of reaching the breakpoint four times, then halting.

Would any of you out there have an idea why counting breakpoints may not be working?  I could really use this
feature to get through some debugging at the moment.

Thanks,
Greg Smith
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,673 次查看
CompilerGuru
NXP Employee
NXP Employee
Works for me with CW 6.1, debugging with a P&E Multilink debugging a S08 QE128.
Note that you have to press Update after changing the interval in the dialog.

Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,674 次查看
CompilerGuru
NXP Employee
NXP Employee
Works for me with CW 6.1, debugging with a P&E Multilink debugging a S08 QE128.
Note that you have to press Update after changing the interval in the dialog.

Daniel
0 项奖励
回复