True Time Simulator Counting Breakpoints Not Working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

True Time Simulator Counting Breakpoints Not Working

ソリューションへジャンプ
2,572件の閲覧回数
GFSmith
Contributor II
Hello,
I'm working with a recent version of Freescale's CodeWarrior Development Studio,
version 5.7.0, build 2211, for the HCS12 processor, specifically the MC9S12E128,
and the True Time Simulator (Version 6.1, Build 6345).

Downloading code, single-stepping through the code, and setting simple
breakpoints is working.  I can't get Counting Breakpoints to work.  I have
followed the directions by setting the interval to say, for example, "4", then
running the code, but the debugger appears to be triggering as soon as it hits
the breakpoint instead of reaching the breakpoint four times, then halting.

Would any of you out there have an idea why counting breakpoints may not be working?  I could really use this
feature to get through some debugging at the moment.

Thanks,
Greg Smith
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,669件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Works for me with CW 6.1, debugging with a P&E Multilink debugging a S08 QE128.
Note that you have to press Update after changing the interval in the dialog.

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,670件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Works for me with CW 6.1, debugging with a P&E Multilink debugging a S08 QE128.
Note that you have to press Update after changing the interval in the dialog.

Daniel
0 件の賞賛
返信