Trimming HCS08 in DEBUG MODE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Trimming HCS08 in DEBUG MODE

跳至解决方案
4,051 次查看
Andrew
Contributor I
Hello,
Does anyone know how to trim the internal clock generator of my HCS08 when run HiWave (Debugger) from CW 5.0?
 
Thanks
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,177 次查看
peg
Senior Contributor IV

Ok, if there is not a similar way then you probably can't do it via CW.

David

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,177 次查看
peg
Senior Contributor IV

Hi Andrew,

If you are using a P&E Multilink or Cyclone...

Under the MultilinkCyclonePro menu

Select "Advanced Programming/Debug Options"

Then make sure there is a tick beside

"Calculate Trim and Programme Non-Volatile Trim Register"

That's it!

Regards David

 

0 项奖励
回复
2,177 次查看
Andrew
Contributor I

No,

I'm using the InDART of the Softec.

 

0 项奖励
回复
2,178 次查看
peg
Senior Contributor IV

Ok, if there is not a similar way then you probably can't do it via CW.

David

 

0 项奖励
回复