Trimming HCS08 in DEBUG MODE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trimming HCS08 in DEBUG MODE

ソリューションへジャンプ
4,080件の閲覧回数
Andrew
Contributor I
Hello,
Does anyone know how to trim the internal clock generator of my HCS08 when run HiWave (Debugger) from CW 5.0?
 
Thanks
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,206件の閲覧回数
peg
Senior Contributor IV

Ok, if there is not a similar way then you probably can't do it via CW.

David

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,206件の閲覧回数
peg
Senior Contributor IV

Hi Andrew,

If you are using a P&E Multilink or Cyclone...

Under the MultilinkCyclonePro menu

Select "Advanced Programming/Debug Options"

Then make sure there is a tick beside

"Calculate Trim and Programme Non-Volatile Trim Register"

That's it!

Regards David

 

0 件の賞賛
返信
2,206件の閲覧回数
Andrew
Contributor I

No,

I'm using the InDART of the Softec.

 

0 件の賞賛
返信
2,207件の閲覧回数
peg
Senior Contributor IV

Ok, if there is not a similar way then you probably can't do it via CW.

David

 

0 件の賞賛
返信