Trimming HCS08 in DEBUG MODE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trimming HCS08 in DEBUG MODE

Jump to solution
4,059 Views
Andrew
Contributor I
Hello,
Does anyone know how to trim the internal clock generator of my HCS08 when run HiWave (Debugger) from CW 5.0?
 
Thanks
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,185 Views
peg
Senior Contributor IV

Ok, if there is not a similar way then you probably can't do it via CW.

David

 

View solution in original post

0 Kudos
Reply
3 Replies
2,185 Views
peg
Senior Contributor IV

Hi Andrew,

If you are using a P&E Multilink or Cyclone...

Under the MultilinkCyclonePro menu

Select "Advanced Programming/Debug Options"

Then make sure there is a tick beside

"Calculate Trim and Programme Non-Volatile Trim Register"

That's it!

Regards David

 

0 Kudos
Reply
2,185 Views
Andrew
Contributor I

No,

I'm using the InDART of the Softec.

 

0 Kudos
Reply
2,186 Views
peg
Senior Contributor IV

Ok, if there is not a similar way then you probably can't do it via CW.

David

 

0 Kudos
Reply