TBDML and CW5.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TBDML and CW5.1

跳至解决方案
2,258 次查看
bricofab
Contributor I
Hello,

I've made a TBDML and I've installed it on my computer but when I use it with a S08QG4, there is no work. I write "set gdi" on the command windows, I configure the good dll but it never work.
Does someone have an experience with TBDML and CW5.1?

Thanks a lot for your help.
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,140 次查看
eckhard
Contributor V
Hello,

TBDML is only for the hcs12 controller family. If you want to programm a mc9s08 controller ou should check OSBDM.

Eckhard

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,141 次查看
eckhard
Contributor V
Hello,

TBDML is only for the hcs12 controller family. If you want to programm a mc9s08 controller ou should check OSBDM.

Eckhard
0 项奖励
回复
1,140 次查看
bricofab
Contributor I
And is OSBDM running with CW5.1? It is noticed that it's running with 5.0 but no informations with 5.1.
 
Thanks for your help.
 
Bricofab
0 项奖励
回复