TBDML and CW5.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,338件の閲覧回数
bricofab
Contributor I
Hello,

I've made a TBDML and I've installed it on my computer but when I use it with a S08QG4, there is no work. I write "set gdi" on the command windows, I configure the good dll but it never work.
Does someone have an experience with TBDML and CW5.1?

Thanks a lot for your help.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,220件の閲覧回数
eckhard
Contributor V
Hello,

TBDML is only for the hcs12 controller family. If you want to programm a mc9s08 controller ou should check OSBDM.

Eckhard

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,221件の閲覧回数
eckhard
Contributor V
Hello,

TBDML is only for the hcs12 controller family. If you want to programm a mc9s08 controller ou should check OSBDM.

Eckhard
0 件の賞賛
返信
1,220件の閲覧回数
bricofab
Contributor I
And is OSBDM running with CW5.1? It is noticed that it's running with 5.0 but no informations with 5.1.
 
Thanks for your help.
 
Bricofab
0 件の賞賛
返信