Support for MC9S12NE64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for MC9S12NE64

Jump to solution
1,716 Views
eddie
Contributor I
Service pack for CW3.1 exists for NE64
No service pack or any kind of support for NE64 in CW4.5
What goes?
Is this part dead?
I just bought expensive MicroNet CMX package for it
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
871 Views
Alban
Senior Contributor II
Hi Eddie,
 
I just tried in my CW4.5 and NE64 is on as standard, you don't need any package.
You needed a service pack for CW3.1 for S12 because CW3.1 was created before the NE64.
 
As CW4.5 for S12 was released quite recently, the NE64 is included. I created an NE64 project with the wizard just now.
 
The part is not dead, and if you look in the 16 board of the Forum, there is actually quite a lot of discussion about it !
 
Cheers,
Alban.

View solution in original post

0 Kudos
Reply
1 Reply
872 Views
Alban
Senior Contributor II
Hi Eddie,
 
I just tried in my CW4.5 and NE64 is on as standard, you don't need any package.
You needed a service pack for CW3.1 for S12 because CW3.1 was created before the NE64.
 
As CW4.5 for S12 was released quite recently, the NE64 is included. I created an NE64 project with the wizard just now.
 
The part is not dead, and if you look in the 16 board of the Forum, there is actually quite a lot of discussion about it !
 
Cheers,
Alban.
0 Kudos
Reply