Support for MC9S12NE64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support for MC9S12NE64

ソリューションへジャンプ
2,452件の閲覧回数
eddie
Contributor I
Service pack for CW3.1 exists for NE64
No service pack or any kind of support for NE64 in CW4.5
What goes?
Is this part dead?
I just bought expensive MicroNet CMX package for it
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,607件の閲覧回数
Alban
Senior Contributor II
Hi Eddie,
 
I just tried in my CW4.5 and NE64 is on as standard, you don't need any package.
You needed a service pack for CW3.1 for S12 because CW3.1 was created before the NE64.
 
As CW4.5 for S12 was released quite recently, the NE64 is included. I created an NE64 project with the wizard just now.
 
The part is not dead, and if you look in the 16 board of the Forum, there is actually quite a lot of discussion about it !
 
Cheers,
Alban.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,608件の閲覧回数
Alban
Senior Contributor II
Hi Eddie,
 
I just tried in my CW4.5 and NE64 is on as standard, you don't need any package.
You needed a service pack for CW3.1 for S12 because CW3.1 was created before the NE64.
 
As CW4.5 for S12 was released quite recently, the NE64 is included. I created an NE64 project with the wizard just now.
 
The part is not dead, and if you look in the 16 board of the Forum, there is actually quite a lot of discussion about it !
 
Cheers,
Alban.
0 件の賞賛
返信