Stepper motor IC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,329件の閲覧回数
admin
Specialist II

hello friends,

 can anyone please suggest me a stepper motor controller IC for automotive application???

 I would also like to ask u what would be the ideal specifications... this is for the first time iam given the work to choose a controller IC.. so, it will be of great help of how do i choose such ICs n what to look in for???

thankyou in advance.. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,794件の閲覧回数
Pivson
Contributor II

Hello, try to check (for example) ST L9935 (http://www.stm.com/stonline/products/literature/ds/5198.pdf). We used these IC's in some automation appz. There are no "ideal" - but features you may need to look for:

 

- delayed channel switch (reduces peak)

- controlled VOUT slope (minimized EMI)

- shortcut prodection

 

etc... Depends on requirements.

 

Pivson

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,795件の閲覧回数
Pivson
Contributor II

Hello, try to check (for example) ST L9935 (http://www.stm.com/stonline/products/literature/ds/5198.pdf). We used these IC's in some automation appz. There are no "ideal" - but features you may need to look for:

 

- delayed channel switch (reduces peak)

- controlled VOUT slope (minimized EMI)

- shortcut prodection

 

etc... Depends on requirements.

 

Pivson

 

0 件の賞賛
返信
1,795件の閲覧回数
vishaka_maithil
Contributor I

Thank you,

though it is a delayed reply, I will follow up the link and update on stepper motor ICs.

:smileyhappy:

0 件の賞賛
返信