Start automatically debugger on CodeWarrior MCU 10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Start automatically debugger on CodeWarrior MCU 10.6

2,482 Views
romainbenet
Contributor III


Hi,

 

for my project I need to load a lot of .elf files (so a lot of different projects) into the same target one after another but automatically into a same script.

 

How can I start this script on CW and how can I reuse default code used for programming the target ?

 

Best regards,

Romain

Labels (1)
0 Kudos
Reply
5 Replies

2,262 Views
BlackNight
NXP Employee
NXP Employee

Hi Romain,

maybe this is what you are looking for: Debugger Shell: Test Automation | MCU on Eclipse

I hope this helps,

Erich

0 Kudos
Reply

2,262 Views
romainbenet
Contributor III

Ok but how can you specify it that you want to load not the current project but another from other wokspace (the elf file exists) ?

Specifically I want to have one global file (global_file.tcl) which begins by call debug mode then debug_file0.tcl, debug_file1.tcl... then exits the debug mode and each debug_filex.tcl loads a specific projects (*.elf file) and executes automatically its goal.

Thanks for your help,

Romain

0 Kudos
Reply

2,262 Views
BlackNight
NXP Employee
NXP Employee

You can load any file from your disk (elf file), you only need to point to the correct .elf file.

0 Kudos
Reply

2,262 Views
romainbenet
Contributor III

How do you do to load any file undo tcl script ? Can you write an example please ?

Because when I start the debug keyword undo CW it loads automatically with current project...

Best regards,

Romain

0 Kudos
Reply

2,262 Views
romainbenet
Contributor III

For trying to resolve my problem I use followings examples:

AN3595.pdf - Basic TCL Scripting with the CodeWarrior (2008)

http://mcuoneclipse.com/2012/08/03/codewarrior-flash-programming-from-a-dos-shell/

http://mcuoneclipse.com/2012/04/12/scripting-the-debugger-shell-getting-started/

My problem is: how can I load a specific project (elf file) for a same project [for example: if my project is "CWTest" then I have "CWTest0.elf, CWTest1.elf...] ? (CWTestx is from the same project but don't have same code).

Other problem: how can I load a .mcp file whereas I work on CW 10.6 eclipse (and not IDE) ? I don't have .mcp project.

Best regards,

Romain

0 Kudos
Reply