Special Edition Code Limits

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Special Edition Code Limits

跳至解决方案
1,741 次查看
cktg1
Contributor I

The linker is giving me an error about code size "L4025: This limited version allows only 16384 bytes of code" but the web site says the code limit is 32k:

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-SPECIAL

 

I have both v5.1 and v6.3 installed on my computer and they both give the same error message.

 

Thanks in advance for any help!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,011 次查看
cktg1
Contributor I

Rename or remove the license.dat file in earlier install subdirectories and restart CW to load the proper license. 

 

(I renamed all the license.dat files on the computer and started CW. I got an error that listed the environment variable CW uses to look for license.dat. The LicensePath includes all previous installs, listed in order. When CW starts, it looks through the installs in order so CW v6.3 was loading with a license from v5.0 which is why I couldn't build code bigger than 16k)

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,011 次查看
J2MEJediMaster
Specialist I

It sounds like the default license is broken, somehow. Please work with the licensing people to correct this. Click here to submit a service request to them. Choose Technical Request for the category and License Issues for the topic.

 

---Tom

0 项奖励
回复
1,012 次查看
cktg1
Contributor I

Rename or remove the license.dat file in earlier install subdirectories and restart CW to load the proper license. 

 

(I renamed all the license.dat files on the computer and started CW. I got an error that listed the environment variable CW uses to look for license.dat. The LicensePath includes all previous installs, listed in order. When CW starts, it looks through the installs in order so CW v6.3 was loading with a license from v5.0 which is why I couldn't build code bigger than 16k)

0 项奖励
回复