Special Edition Code Limits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Special Edition Code Limits

Jump to solution
2,619 Views
cktg1
Contributor I

The linker is giving me an error about code size "L4025: This limited version allows only 16384 bytes of code" but the web site says the code limit is 32k:

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-SPECIAL

 

I have both v5.1 and v6.3 installed on my computer and they both give the same error message.

 

Thanks in advance for any help!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,889 Views
cktg1
Contributor I

Rename or remove the license.dat file in earlier install subdirectories and restart CW to load the proper license. 

 

(I renamed all the license.dat files on the computer and started CW. I got an error that listed the environment variable CW uses to look for license.dat. The LicensePath includes all previous installs, listed in order. When CW starts, it looks through the installs in order so CW v6.3 was loading with a license from v5.0 which is why I couldn't build code bigger than 16k)

View solution in original post

0 Kudos
Reply
2 Replies
1,889 Views
J2MEJediMaster
Specialist I

It sounds like the default license is broken, somehow. Please work with the licensing people to correct this. Click here to submit a service request to them. Choose Technical Request for the category and License Issues for the topic.

 

---Tom

0 Kudos
Reply
1,890 Views
cktg1
Contributor I

Rename or remove the license.dat file in earlier install subdirectories and restart CW to load the proper license. 

 

(I renamed all the license.dat files on the computer and started CW. I got an error that listed the environment variable CW uses to look for license.dat. The LicensePath includes all previous installs, listed in order. When CW starts, it looks through the installs in order so CW v6.3 was loading with a license from v5.0 which is why I couldn't build code bigger than 16k)

0 Kudos
Reply