Software analysis/trace for HCS08

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software analysis/trace for HCS08

1,828件の閲覧回数
bob_walker
Contributor III

For some reason, the P&E debugger won't download when I enable trace/software analysis. I get a "An internal error occurred during...." error message. At startup, I'm always greeted with "There is a mismatch between the System environment and the workbench environment, which may result in Software Analysis malfunctioning." I suspect that this is the case. Has anyone seen this one before? Any solution? Any idea where to look?

Perhaps and environment variable is whacked?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,646件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

Windows or Linux host? Which version (10.2 or 10.3)?

Have you just installed a service pack or an update? I have seen such a thing if I do a 'restart' of Eclipse instead of closing it and then start a fresh one.

Not sure, but it could be related to the LD_LIBRARY_PATH (or similar). Could you check/post the content of your cwide-env file (located in the eclipse folder) and check if all the paths exist on your system?

I hope this helps,

Erich

0 件の賞賛
返信

1,646件の閲覧回数
bob_walker
Contributor III

Erich,

That would be Linux (Mageia 32-bit), CW10.2. I'll check my cwide-env file later this evening.

I just checked it on WinXP, CW10.2, and was able to run one analysis.

Bob

0 件の賞賛
返信