CodeWarrior 10.2 SE bareboard project problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 10.2 SE bareboard project problems

1,558 Views
Rob23
Contributor I

If I choose just C only and not include assembly during the new bareboard project config, main.c is not created and also processor expert can not be used. I.e clicking on the mcu items on target cpu image will not open the device initialisation dialogs. If asm support is included main.c and asm_main.asm are created and PE works as expected. Ok it's no big deal to include asm even if not needed but it does seem like a bug to me.

 

I'm using S08JM and S08SH mcu's.

 

Any thoughts?

 

Rob

Labels (1)
0 Kudos
Reply
1 Reply

1,359 Views
Monica
Senior Contributor III

Hey Rob!

Let me see if I got this the right way...PE won't seem to be working if there is not the generation of asm files right?

What CodeWarrior are you using for those MCUs?

0 Kudos
Reply