I'm using a M54451EVB development board. I'm asked for the derivative or board I would like to use:
However, it is unable to find my board. In fact, when I expand all the options, it doesn't look like there are any boards in there.
Is there a way to set up a project to use the a specific dev board, particularly the M54451EVB?
Thank you.
Hi
You create a "New bare board project" which doesn't support selecting board as target, thus you can select chip dirivative only. The "board" you highlighted confuses users. I will report it.
If user use SDK or MQX, board can be selected. but we need check if the SDK or MQX supports this board.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Zachary
yes, MQX is RTOS.
See SDK here
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, MCUXpresso doesn't support codefire.
you use Coldfire M54451EVB , you need use CodWarrior. I just checked MQX doesn't support his board.
As I know we do not have any plan for MQX to support M54451EVB.(Only the M54455EVB are supported in MQX4.x.)
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
If don't use MQX, we can only choose "derivative" only.