Reg: DSC flash programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reg: DSC flash programmer

Jump to solution
1,258 Views
dharanidevimani
Contributor I

Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMMER_V1.2_WIN32 file, We purchased a new laptop with 64-bit version. So its not getting supported. Please help me on this

Labels (1)
0 Kudos
Reply
1 Solution
1,125 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Refer to Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMME...


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,126 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Refer to Is the flash programmer of DSC 56800E is available for Windows 64-bit version?. I have FLSHPROGRAMME...


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply