Re:encryption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re:encryption

1,574件の閲覧回数
guochunhua
Contributor II

Hi

您好!

我不能连接上,你们发给我的链接地址,请你们直接把CAN'的例子程序发给我。我的程序现在就剩下CAN的程序了,没有CAN的程序,不能上车做实验。

 

If you would like to use FlexCAN component ,  please first get its license.

 

http://tinyurl.com/zp3ltgj

 

! I also attached two example projects for FlexCAN which are not based on PE.

 

祝好!

 

 

 

 

 

 

At 2016-06-27 16:11:51, "guochunhua" <[email protected]> wrote:

 

Dear sir

       I want to encrypt the MCU of 56f84789 in PE of codewarrior 10.4, if 56f84789 is locked and I want to reload program to it, what can I do? how can I encrypt and decrypt 56f84789 in PE of codewarrior 10.4?   thank you very much.

 

Best regards.

guo chunhua

ラベル(1)
0 件の賞賛
返信
1 返信

1,421件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Chunhua

I attached an example project for 56F84789 FlexCAN module, which is based on Processor Expert. 

For the project without PE, you can find it in:

https://community.nxp.com/message/651115#comment-651115 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信