Programming Kinetis K10DN512VLL10 with Cyclone Max

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming Kinetis K10DN512VLL10 with Cyclone Max

4,770件の閲覧回数
nvedel
Contributor II

I'm having problems programming Kinetis K10DN512VLL10 with Cyclone Max.

 

I've testet the Cyclone Max with a Freescale K60 tower, where it worked.

 

I'm using CodeWarrior for development and debug, but I have also tried the Cyclone Max in stand-alone mode, where I can save an image, but I can't get it to program my target (I get Error $0007 - Error entering debug mode)

 

My K10 target is a new board I've designed. You can see the JTAG schematic here:

13681_13681.pngJTAG connector schematic.png

 

I have connected a logic analyzer to the JTAG pins and I can see some communication on all lines, but I'm not quite sure what to look after.

It looks like the communication stop after a short while.

The activity can be seen here:

From CodeWarrier:

13682_13682.pngCodeWarrior complete sequence.png

When I press Abort in P&E Connection Assistant, I get these details:

Error launching SS-test-1_FLASH_PnE Cyclone MAX

ARM GDI Protocol Adapter : Can't connect. The Debugger can not connect to the P&E device

 

Stand-alone:

13683_13683.pngStand-alone complete sequence.png

 

 

Setup can be seen here:

CodeWarrior:

13684_13684.pngCodeWarrior setup.png

Stand-alone:

13685_13685.pngStand-alone (SAM) setup.png

 

 

 

 

Does anyone have an idea of what is going wrong?

...or what I should be looking for?

ラベル(1)
5 返答(返信)

3,324件の閲覧回数
takaoyamada
Contributor IV

Greetings,

From looking at your connection settings, you created your own "SS-test-1_Flash" target. Try creating a default project for the K10DN512 and see if you are able to compile and debug a simple project. If this works, then we know somewhere in your connection settings is causing this issue. If it fails as well, then you may have a hardware issue.

Within the Cyclone Max Image creation utility, make sure to specify the communication mode correctly. Are you sure you are not using the 20-pin mini cable on the JTAG/SWD adapter board?

Takao Yamada

P&E Microcomputer Systems

0 件の賞賛
返信

3,324件の閲覧回数
nvedel
Contributor II

Hi Takao

Thanks for answering.

I've tried to create a new project as you suggested:

These are my exact steps:

File - New project

  Codewarrior - Bareboard project

  Name it SS-test-2, using default location

  Select MK10DN512 - Check application

  Connection to be used: P&E Cyclone

  Language: C - Floating point: Software - ARM Build Tools: Freescale

  Rapid Application Development: Processor Expert - Start with perspective designed for: Hardware configuration - Project mode: Standalone

  Finish

Pop-up: Open associated perspective: C/C++ - answer Yes

Click on the new project in "CodeWarrior Projects": SS-test-2 : RAM

Switch to Hardware perspective

   Change CPU type to MK10DN512VLL10 (the one I use)

Project - Generate Processor Expert Code

Press F11 to debug

   Pop-up: Select configuration: - Selects SS-test-2_RAM_PnE Cyclone MAX

CodeWarrior starts Building

CodeWarrior tryes to launch, but fails (P&E Connection Assistant)...

Cyclone Max Image creation utility:

Communication is set to ARM CORTEX 20 PIN and I'm using 20pin, 100mil connector as shown in schematic.

I'm NOT using the adaptor board.



It's very possible that there are a Hardware problem in my board, but I've spend several days looking for it and I can't see the problem myself.

It would be nice, if there was a way to get information on what has went wrong (some kind of log) instead of just a message saying "somethings wrong"


As far as I can see from the datalogger, there are some communication going on, but for some reason it stops.

The first part of the JTAG communication seems to take place, while Reset is held low - is that normal?



0 件の賞賛
返信

3,324件の閲覧回数
nvedel
Contributor II

Update:

I went back to the Tower project, that I'd previously been working on.

Connected the Cyclone Max to the JTAG port and tested that I could still debug. This went fine.

I then created a new project, exactly as described above, only with the MK60DN512VMD10 processor of the TOWER instead of my K10

Now I get the same problem - programmer will not connect.

This leads me to the conclusion that something is wrong in the SW setup - but what?

One should think that it would be easy, when I have one setting that works and one that doesn't, but I havn't seen the light yet...

0 件の賞賛
返信

3,324件の閲覧回数
thomaskang-b295
NXP Employee
NXP Employee

Hi,

Maybe it can help you because I had similar problem, then it was cleared.

Please short pin 7 and 13 of 20-pin connector as below.

Untitled.png

I double checked to P&EMicro and got the answer.

The Cyclone Max was designed prior to the existence of SWD. Because it was designed prior to SWD, the TMS/SWDIO pin is not bidrectional. To support SWD, we included a SWD/JTAG adapter to short TMS/SWDIO with pin 13. Our Cyclone Universal, which is our next Cyclone Product, will not require an adapter and will support SWD mode natively.

Hope it can help.

3,324件の閲覧回数
jorgesierra
Contributor II

We should also mention that the short on the connector is NOT present on the board side of things.

Cyclone     Board

TMS          TMS

TDO          TMS

TDO on the Board side DOESN'T connect to anything! This is very important and it took 2 weeks of my life.

0 件の賞賛
返信