Processor Expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert

Jump to solution
4,124 Views
Tommy44
Contributor III

What version of Code Warrior do I need to purchase to use Processor Expert?  In new project creation with the special edition the Processor Expert option is grayed out.

Labels (1)
0 Kudos
Reply
1 Solution
3,909 Views
Tommy44
Contributor III

It does work after a reboot, but what I was talking about was New -->

Bareboard project, select Kinetis L, --> KL25 etc, then Select Open SDA,

then Rapid Application Development, would not allow Processor Expert to

be selected. Thanks for the info about the license!

View solution in original post

0 Kudos
Reply
6 Replies
3,909 Views
BlackNight
NXP Employee
NXP Employee

You need at least the Free Community Edition license (free of charge). For MCU10.3 you have to install it manually. See

Getting Started · ErichStyger/mcuoneclipse Wiki · GitHub

how to install that license.

0 Kudos
Reply
3,909 Views
Tommy44
Contributor III

Thanks for the reply. I copied the text to a file, license.dat and

copied it into the /installpath/mcu directory, but I still can not

enable Processor Expert in new project creation. Did I leave out anything?

0 Kudos
Reply
3,909 Views
BlackNight
NXP Employee
NXP Employee

Hello Thomas,

are we talking about the same thing?

The menu File > New > Embedded Component Project

?

Or what new project creation do you mean?

0 Kudos
Reply
3,910 Views
Tommy44
Contributor III

It does work after a reboot, but what I was talking about was New -->

Bareboard project, select Kinetis L, --> KL25 etc, then Select Open SDA,

then Rapid Application Development, would not allow Processor Expert to

be selected. Thanks for the info about the license!

0 Kudos
Reply
3,909 Views
BlackNight
NXP Employee
NXP Employee

so everything is fine for you now?

You should not need to reboot (maybe restart eclipse, but not reboot).

Otherwise: if a microcontroller is not supported with Processor Expert, then I would as well expect that the option is grayed out. But the KL25Z is definitely supported.

Anyway. Good if it is working now on your end. Can you confirm.

0 Kudos
Reply
3,909 Views
Tommy44
Contributor III

Yes, works fine now. Thank you.

0 Kudos
Reply