Processor Expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,330件の閲覧回数
Tommy44
Contributor III

What version of Code Warrior do I need to purchase to use Processor Expert?  In new project creation with the special edition the Processor Expert option is grayed out.

ラベル(1)
0 件の賞賛
返信
1 解決策
4,115件の閲覧回数
Tommy44
Contributor III

It does work after a reboot, but what I was talking about was New -->

Bareboard project, select Kinetis L, --> KL25 etc, then Select Open SDA,

then Rapid Application Development, would not allow Processor Expert to

be selected. Thanks for the info about the license!

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,115件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You need at least the Free Community Edition license (free of charge). For MCU10.3 you have to install it manually. See

Getting Started · ErichStyger/mcuoneclipse Wiki · GitHub

how to install that license.

0 件の賞賛
返信
4,115件の閲覧回数
Tommy44
Contributor III

Thanks for the reply. I copied the text to a file, license.dat and

copied it into the /installpath/mcu directory, but I still can not

enable Processor Expert in new project creation. Did I leave out anything?

0 件の賞賛
返信
4,115件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello Thomas,

are we talking about the same thing?

The menu File > New > Embedded Component Project

?

Or what new project creation do you mean?

0 件の賞賛
返信
4,116件の閲覧回数
Tommy44
Contributor III

It does work after a reboot, but what I was talking about was New -->

Bareboard project, select Kinetis L, --> KL25 etc, then Select Open SDA,

then Rapid Application Development, would not allow Processor Expert to

be selected. Thanks for the info about the license!

0 件の賞賛
返信
4,115件の閲覧回数
BlackNight
NXP Employee
NXP Employee

so everything is fine for you now?

You should not need to reboot (maybe restart eclipse, but not reboot).

Otherwise: if a microcontroller is not supported with Processor Expert, then I would as well expect that the option is grayed out. But the KL25Z is definitely supported.

Anyway. Good if it is working now on your end. Can you confirm.

0 件の賞賛
返信
4,115件の閲覧回数
Tommy44
Contributor III

Yes, works fine now. Thank you.

0 件の賞賛
返信