Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Processor Expert

跳至解决方案
4,284 次查看
Tommy44
Contributor III

What version of Code Warrior do I need to purchase to use Processor Expert?  In new project creation with the special edition the Processor Expert option is grayed out.

标签 (1)
0 项奖励
回复
1 解答
4,069 次查看
Tommy44
Contributor III

It does work after a reboot, but what I was talking about was New -->

Bareboard project, select Kinetis L, --> KL25 etc, then Select Open SDA,

then Rapid Application Development, would not allow Processor Expert to

be selected. Thanks for the info about the license!

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,069 次查看
BlackNight
NXP Employee
NXP Employee

You need at least the Free Community Edition license (free of charge). For MCU10.3 you have to install it manually. See

Getting Started · ErichStyger/mcuoneclipse Wiki · GitHub

how to install that license.

0 项奖励
回复
4,069 次查看
Tommy44
Contributor III

Thanks for the reply. I copied the text to a file, license.dat and

copied it into the /installpath/mcu directory, but I still can not

enable Processor Expert in new project creation. Did I leave out anything?

0 项奖励
回复
4,069 次查看
BlackNight
NXP Employee
NXP Employee

Hello Thomas,

are we talking about the same thing?

The menu File > New > Embedded Component Project

?

Or what new project creation do you mean?

0 项奖励
回复
4,070 次查看
Tommy44
Contributor III

It does work after a reboot, but what I was talking about was New -->

Bareboard project, select Kinetis L, --> KL25 etc, then Select Open SDA,

then Rapid Application Development, would not allow Processor Expert to

be selected. Thanks for the info about the license!

0 项奖励
回复
4,069 次查看
BlackNight
NXP Employee
NXP Employee

so everything is fine for you now?

You should not need to reboot (maybe restart eclipse, but not reboot).

Otherwise: if a microcontroller is not supported with Processor Expert, then I would as well expect that the option is grayed out. But the KL25Z is definitely supported.

Anyway. Good if it is working now on your end. Can you confirm.

0 项奖励
回复
4,069 次查看
Tommy44
Contributor III

Yes, works fine now. Thank you.

0 项奖励
回复