Processor Expert CW10.6 Error Message on MKE06Z ConsoleIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Processor Expert CW10.6 Error Message on MKE06Z ConsoleIO

跳至解决方案
1,856 次查看
eyeow84
Contributor III

I am currently using FRDM-KE06Z (MKE06Z128VLK4) with CW 10.6. I am trying to use the Processor Expert (PE) to configure and generate code for the console for communication with my PC hyperterminal. Before that I was utilizing the sample codes from FRDM-KEXX Driver Library Package and the communication at hyperterminal works fine. And I understand that those sample codes is not generated from Processor Expert.

 

After I have setup the bareboard project folder based on target MCU MKE06Z128VLK4, next I wanted to go to component library of PE to select consoleIO and configure it. However error message below shown out:

 

Error: Error in the inherited component settings

 

It seems like I wasn't allowed to further configure this consoleIO. May I know why is this happening? or did I miss out something?

 

Thanks.

 

170437_170437.jpgProcessor selection Component Library.jpg

.170436_170436.jpgPE consoleIO error message.jpg

170435_170435.jpgPE consoleIO doesn't have option to choose.jpg

标签 (1)
0 项奖励
回复
1 解答
1,650 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eyoew,

Please configure the Serial_ LDD component refer to your board, which UART, baud rate and other conifugrations:

pastedImage_1.png

Hope it hepls


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,651 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eyoew,

Please configure the Serial_ LDD component refer to your board, which UART, baud rate and other conifugrations:

pastedImage_1.png

Hope it hepls


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,650 次查看
eyeow84
Contributor III

Hi Alice,

Thanks for your advice. I think the error message has gone and PE code can be generated. But whether do you why I cannot specifically configure 115200 baud rate? Thanks...baud rate 115200 disallowed.jpg

0 项奖励
回复