Processor Expert - Add

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert - Add

2,563 Views
ronaldpatton
Contributor I

Hello,

 

I am attempting to add a component to an existing project using the processor expert facility.  The component is an I2C component.  When I right click on the component in an attempt to add it to the existing project the "add to project" is greyed out.

 

What am I doing wrong or is this yet another issue with Code Warrior 10.6?

 

I have attached the project.

Original Attachment has been moved to: project.zip

Labels (1)
0 Kudos
Reply
4 Replies

2,318 Views
trytohelp
NXP Employee
NXP Employee

Hi Ronald,

The project sent doesn't include Processor Expert.

I've created a project based on mc9s08qg8 with the wizard including Processor Expert.

I can add the InternalI2C bean without problem and build the project.

I'm using CW for MCU v10.6.4 +Patch 10.6.5 which is the last version.

Attached you will find the example.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,318 Views
ronaldpatton
Contributor I

Hi,

OK, I have brought up the test project, but the chip is wrong.   Your test project has MC9S08QG8CFK.  I need MC9S08QG8CPBE

Regards,

Ron Patton

0 Kudos
Reply

2,318 Views
trytohelp
NXP Employee
NXP Employee

Hi Ron,

You can change the device in the project sent or ...

I've created a new project for QG8 and changed the device.

To do that, click on Components Library and select the processor family: HCS08 - QA/QD/QG - MC9S08QG8.

Now in the dialog you can select the MC9S08QG8CPB.

pastedImage_0.png

Then I added the InternalI2C bean.

Attached the new project.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,318 Views
ronaldpatton
Contributor I

OK, thanks.  That worked.  Now I will determine if the existing project source code will compile and build.

Regards,

Ron Patton

0 Kudos
Reply