Problem with CW10.5  he used 56F8323

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem with CW10.5  he used 56F8323

跳至解决方案
2,706 次查看
PitOn
Contributor III

Problem with CW10.5  he used 56F8323 with CW classic and his project worked great.

  After upgrading CW t o10.5(10.4 and lower don't support import  from CW classic) during debug MCU flash is not initialized,

but if  customer use programmer mode everything works ok.   Debug probe is USB-TAP.

标签 (1)
0 项奖励
回复
1 解答
2,356 次查看
TICS_Fiona
NXP Employee
NXP Employee

The problem in your debuggin is different. I will answer it in SR.

在原帖中查看解决方案

10 回复数
2,356 次查看
TICS_Fiona
NXP Employee
NXP Employee

Would you please create a new project for your target from <File> menu -> New->Bareboard project, can CodeWarrior v10.5 program with this project into your project?

If it can, please compare its debugger settings in Project Properties with your project, especially whether the initialization file and memory file are selected correctly.

initialization&memory file.png

0 项奖励
回复
2,356 次查看
uSasha
Contributor II

Hello Fiona, i have the same problem.

I opened a service request number 1-1179943257.

The problem happens only with USB-TAP.

Multilink works perfectly.

0 项奖励
回复
2,357 次查看
TICS_Fiona
NXP Employee
NXP Employee

The problem in your debuggin is different. I will answer it in SR.

2,356 次查看
PitOn
Contributor III

Hi Fiona, the exact same problem. I asked Alexander to initiate SR.

0 项奖励
回复
2,356 次查看
Ben
Senior Contributor I

Hi Konstantin and Aleksander

I had a similar problem with the USBTAP, and after adding the tcl file location as Fiona noted and updating the memory file too, it started to work good. Try it

0 项奖励
回复
2,356 次查看
Ben
Senior Contributor I

Konstantin, I have to add that I still had other problems with 10.5 and re-installed 10.4.

I am waiting for a new version or patch.

About importing old project to 10.4: there is AN4727 about how to do it.

0 项奖励
回复
2,356 次查看
PitOn
Contributor III

Thank you Ben. I need to convert about one hundred projects.:smileyshocked:

0 项奖励
回复
2,356 次查看
PitOn
Contributor III

I'm talking about the USB TAP, as an example MULTILINK.

Does not work with USB TAP.

0 项奖励
回复
2,356 次查看
TICS_Fiona
NXP Employee
NXP Employee

The same options are also there in Multlink connection settings.

0 项奖励
回复
2,356 次查看
PitOn
Contributor III

Everything is done. The problem remained.

0 项奖励
回复