Problem with CW10.5  he used 56F8323

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with CW10.5  he used 56F8323

Jump to solution
2,643 Views
PitOn
Contributor III

Problem with CW10.5  he used 56F8323 with CW classic and his project worked great.

  After upgrading CW t o10.5(10.4 and lower don't support import  from CW classic) during debug MCU flash is not initialized,

but if  customer use programmer mode everything works ok.   Debug probe is USB-TAP.

Labels (1)
0 Kudos
Reply
1 Solution
2,293 Views
TICS_Fiona
NXP Employee
NXP Employee

The problem in your debuggin is different. I will answer it in SR.

View solution in original post

10 Replies
2,293 Views
TICS_Fiona
NXP Employee
NXP Employee

Would you please create a new project for your target from <File> menu -> New->Bareboard project, can CodeWarrior v10.5 program with this project into your project?

If it can, please compare its debugger settings in Project Properties with your project, especially whether the initialization file and memory file are selected correctly.

initialization&memory file.png

0 Kudos
Reply
2,293 Views
uSasha
Contributor II

Hello Fiona, i have the same problem.

I opened a service request number 1-1179943257.

The problem happens only with USB-TAP.

Multilink works perfectly.

0 Kudos
Reply
2,294 Views
TICS_Fiona
NXP Employee
NXP Employee

The problem in your debuggin is different. I will answer it in SR.

2,293 Views
PitOn
Contributor III

Hi Fiona, the exact same problem. I asked Alexander to initiate SR.

0 Kudos
Reply
2,293 Views
Ben
Senior Contributor I

Hi Konstantin and Aleksander

I had a similar problem with the USBTAP, and after adding the tcl file location as Fiona noted and updating the memory file too, it started to work good. Try it

0 Kudos
Reply
2,293 Views
Ben
Senior Contributor I

Konstantin, I have to add that I still had other problems with 10.5 and re-installed 10.4.

I am waiting for a new version or patch.

About importing old project to 10.4: there is AN4727 about how to do it.

0 Kudos
Reply
2,293 Views
PitOn
Contributor III

Thank you Ben. I need to convert about one hundred projects.:smileyshocked:

0 Kudos
Reply
2,293 Views
PitOn
Contributor III

I'm talking about the USB TAP, as an example MULTILINK.

Does not work with USB TAP.

0 Kudos
Reply
2,293 Views
TICS_Fiona
NXP Employee
NXP Employee

The same options are also there in Multlink connection settings.

0 Kudos
Reply
2,293 Views
PitOn
Contributor III

Everything is done. The problem remained.

0 Kudos
Reply