Problem with CW v10.3, printf and MC56F84789

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with CW v10.3, printf and MC56F84789

ソリューションへジャンプ
1,246件の閲覧回数
fb1
Contributor I

Hi,

 

I am using CW v10.3 SE with a MC56F84789 micro. When i use processor expert AND printf, the debugger hangs at 99% while loading the micro, however if i create a blank project without PE and utilize printf, the entire binary loads and i am able to use the debugger. Any suggestions will be greatly appreciate. Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,119件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Since you are using Special Edition, I would recommend updating to CW10.5, it can be downloaded from:

http://tinyurl.com/6jo5tge

If the problem still exist, please attach your project.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,120件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Since you are using Special Edition, I would recommend updating to CW10.5, it can be downloaded from:

http://tinyurl.com/6jo5tge

If the problem still exist, please attach your project.

0 件の賞賛
返信
1,119件の閲覧回数
fb1
Contributor I

v10.5 worked, thanks!

0 件の賞賛
返信