Problem with CW v10.3, printf and MC56F84789

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem with CW v10.3, printf and MC56F84789

跳至解决方案
1,232 次查看
fb1
Contributor I

Hi,

 

I am using CW v10.3 SE with a MC56F84789 micro. When i use processor expert AND printf, the debugger hangs at 99% while loading the micro, however if i create a blank project without PE and utilize printf, the entire binary loads and i am able to use the debugger. Any suggestions will be greatly appreciate. Thanks!

标签 (1)
0 项奖励
回复
1 解答
1,105 次查看
TICS_Fiona
NXP Employee
NXP Employee

Since you are using Special Edition, I would recommend updating to CW10.5, it can be downloaded from:

http://tinyurl.com/6jo5tge

If the problem still exist, please attach your project.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,106 次查看
TICS_Fiona
NXP Employee
NXP Employee

Since you are using Special Edition, I would recommend updating to CW10.5, it can be downloaded from:

http://tinyurl.com/6jo5tge

If the problem still exist, please attach your project.

0 项奖励
回复
1,105 次查看
fb1
Contributor I

v10.5 worked, thanks!

0 项奖励
回复