Problem programming the MC13213-SRB with BDM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem programming the MC13213-SRB with BDM

Jump to solution
3,029 Views
hauptman
Contributor I
Hi!

I've got a MC13213-SRB board and want to connect it via BDM to CodeWarrior.
When I start hiwave.exe and set connection to HCS08 on P&E Multilink it doesn't detect any known ports ... I've connected the SRB board to my PC via the given USB cable.

Don't know what to do, I've already read the help but it doesn't help me x.x however, other function like the embedded bootloader or the triax tool work fine via USB.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,084 Views
J2MEJediMaster
Specialist I
OK, when you plug the board into the USB cable and then into the PC, does:

1) The PC acknowledge that a USB device was attached? (For Windows XP you get one of those little text bubbles, or it makes a "ding-dong" sound?)

2) Do any LEDs light up on the board? Typically, on most boards you'll get a yellow LED glow for board power and a green or blue LED glow for USB communications.

---Tom

View solution in original post

0 Kudos
Reply
2 Replies
2,085 Views
J2MEJediMaster
Specialist I
OK, when you plug the board into the USB cable and then into the PC, does:

1) The PC acknowledge that a USB device was attached? (For Windows XP you get one of those little text bubbles, or it makes a "ding-dong" sound?)

2) Do any LEDs light up on the board? Typically, on most boards you'll get a yellow LED glow for board power and a green or blue LED glow for USB communications.

---Tom
0 Kudos
Reply
2,084 Views
hauptman
Contributor I
Hi!

Well, I think I found the problem x.x something is broken hmm I think I need to use the embedded bootloader instead (this works fine)
0 Kudos
Reply