Problem programming the MC13213-SRB with BDM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem programming the MC13213-SRB with BDM

跳至解决方案
2,138 次查看
hauptman
Contributor I
Hi!

I've got a MC13213-SRB board and want to connect it via BDM to CodeWarrior.
When I start hiwave.exe and set connection to HCS08 on P&E Multilink it doesn't detect any known ports ... I've connected the SRB board to my PC via the given USB cable.

Don't know what to do, I've already read the help but it doesn't help me x.x however, other function like the embedded bootloader or the triax tool work fine via USB.
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,193 次查看
J2MEJediMaster
Specialist I
OK, when you plug the board into the USB cable and then into the PC, does:

1) The PC acknowledge that a USB device was attached? (For Windows XP you get one of those little text bubbles, or it makes a "ding-dong" sound?)

2) Do any LEDs light up on the board? Typically, on most boards you'll get a yellow LED glow for board power and a green or blue LED glow for USB communications.

---Tom

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,194 次查看
J2MEJediMaster
Specialist I
OK, when you plug the board into the USB cable and then into the PC, does:

1) The PC acknowledge that a USB device was attached? (For Windows XP you get one of those little text bubbles, or it makes a "ding-dong" sound?)

2) Do any LEDs light up on the board? Typically, on most boards you'll get a yellow LED glow for board power and a green or blue LED glow for USB communications.

---Tom
0 项奖励
回复
1,193 次查看
hauptman
Contributor I
Hi!

Well, I think I found the problem x.x something is broken hmm I think I need to use the embedded bootloader instead (this works fine)
0 项奖励
回复