Problem in the flash of a mc9s08pl4 with usbdm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in the flash of a mc9s08pl4 with usbdm

1,868件の閲覧回数
Floppy01
Contributor I

Good morning,

I wanted to program a mc9s08pl4, after writing a simple program I compiled and clicked on debug, the debugger cannot connect with the microcontroller, the error I get 'CORBA connection error'. I use usbdm. Can anyone help me?Immagine.png

This is the code I wrote:

Floppy01_0-1625227538379.png

Thank you!

0 件の賞賛
返信
3 返答(返信)

1,861件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

 Is this a custom board?

 

Can you check that the DBM lines are correct, reset is correct, BKGD pin us plugged, VDD and GND 

 

Regards

Vicente G

0 件の賞賛
返信

1,855件の閲覧回数
Floppy01
Contributor I

Yes, I mounted the mcu on the breadboard and connected the usbdm, the following is the circuit diagram:

Floppy01_1-1625303277079.png

 

i checked the connection, they are both connected also because i tried the same circuit with a qg8 and it works.

 

0 件の賞賛
返信

1,839件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Can you check if the reset line is holding in low? did you see any signal on the BKGB line?

 

Please check all the connections, I am not sure if your USBDM is able to provide power to the board or if you also need to add power to the board.

 

Regards

 

0 件の賞賛
返信