Problem in the flash of a mc9s08pl4 with usbdm

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem in the flash of a mc9s08pl4 with usbdm

1,839 次查看
Floppy01
Contributor I

Good morning,

I wanted to program a mc9s08pl4, after writing a simple program I compiled and clicked on debug, the debugger cannot connect with the microcontroller, the error I get 'CORBA connection error'. I use usbdm. Can anyone help me?Immagine.png

This is the code I wrote:

Floppy01_0-1625227538379.png

Thank you!

0 项奖励
回复
3 回复数

1,832 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

 Is this a custom board?

 

Can you check that the DBM lines are correct, reset is correct, BKGD pin us plugged, VDD and GND 

 

Regards

Vicente G

0 项奖励
回复

1,826 次查看
Floppy01
Contributor I

Yes, I mounted the mcu on the breadboard and connected the usbdm, the following is the circuit diagram:

Floppy01_1-1625303277079.png

 

i checked the connection, they are both connected also because i tried the same circuit with a qg8 and it works.

 

0 项奖励
回复

1,810 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Can you check if the reset line is holding in low? did you see any signal on the BKGB line?

 

Please check all the connections, I am not sure if your USBDM is able to provide power to the board or if you also need to add power to the board.

 

Regards

 

0 项奖励
回复