Problem With CW_MCUs_V6_0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem With CW_MCUs_V6_0

Jump to solution
2,799 Views
Gabo
Contributor I
Hello, I´m trying to use the evaluation version of cw 6.0 for microcontrollers, especially hc08 and hc12 and i´ve downloaded from freescale page, evaluation version, and downloaded the license.dat too, installed the program, placed the license in the installation path and wheni started the program, started a project and clicked on set (to place the path to save the project) the program just closed, it happened without setting the path too, when i click on next to start the project it closed too. I tryed to install it on other computers, downloading licences for them too and it happened all the same.
What should i do?
Thanks
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,846 Views
CompilerGuru
NXP Employee
NXP Employee
read this thread
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...

Basically there is a incompatibility of MS Groove with anything running in a Windows 2000 compatibility mode.

Daniel

View solution in original post

0 Kudos
Reply
2 Replies
1,847 Views
CompilerGuru
NXP Employee
NXP Employee
read this thread
http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...

Basically there is a incompatibility of MS Groove with anything running in a Windows 2000 compatibility mode.

Daniel
0 Kudos
Reply
1,846 Views
Gabo
Contributor I
Thank You, it solved my problem.
Gabriel
0 Kudos
Reply