Option __FILE__ for compiler HC12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Option __FILE__ for compiler HC12

ソリューションへジャンプ
2,323件の閲覧回数
DavidSouche
Contributor I

Hi,

 

I'm a french software designer. I work in embedded system for lift.

 

I develop on a Freescale MC9S.

In my soft, I use option __FILE__ of compiler HC12. This option give me the complete path of my file, but I just want the name of my file and not the path. 

Is there another compiler option to get the short name of a file?

 

Thank you.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,693件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee

I'm not aware of an option for this purpose.

I have to admit that I did look for the same topic in another compiler once too :smileysad:.

(I did not find it there either).

 

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,694件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee

I'm not aware of an option for this purpose.

I have to admit that I did look for the same topic in another compiler once too :smileysad:.

(I did not find it there either).

 

Daniel

0 件の賞賛
返信