OS Upgrade

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OS Upgrade

Jump to solution
3,105 Views
stp1200
Contributor I
If we upgrade our operating system from Windows 2000 to Windows XP, can we use the same license file when we reinstall Codewarrior on XP?

I'm using Codewarrior 3.1 for the HCS12, single user license (no usb dongle).

Thanks,
-shane
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,588 Views
BlackNight
NXP Employee
NXP Employee
Hello,
yes, Codewarrior licenses are independent from the Windows version (XP, XP home, 2000, etc).

Erich

View solution in original post

0 Kudos
Reply
1 Reply
1,589 Views
BlackNight
NXP Employee
NXP Employee
Hello,
yes, Codewarrior licenses are independent from the Windows version (XP, XP home, 2000, etc).

Erich
0 Kudos
Reply